lpcxpresso and mbed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpcxpresso and mbed

1,454 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mayotte1 on Tue Jan 12 09:32:35 MST 2010
If we cut apart the lpcxpresso board, can we plug in the mbed board and used the lpcxpresso debug tools and treat the mbed as just another lpc1768 board?
0 Kudos
Reply
3 Replies

1,412 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Sun Jan 24 23:18:13 MST 2010

Quote: mayotte1
If we cut apart the lpcxpresso board, can we plug in the mbed board and used the lpcxpresso debug tools and treat the mbed as just another lpc1768 board?



The mbed board does not have debugger connections on it, so it cannot be connected to an external debugger such as the LPCXpresso LPC-LINK. However the LPCXpresso IDE can generate binary files which can be programmed into the mbed board over the USB connection.
0 Kudos
Reply

1,412 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by annodomini2 on Tue Jan 19 14:31:03 MST 2010

Quote: mayotte1
If we cut apart the lpcxpresso board, can we plug in the mbed board and used the lpcxpresso debug tools and treat the mbed as just another lpc1768 board?



You can't access the JTAG pins on the mbed as they are used by the 'magic' chip to program the LPC1768 on reset of the mbed
0 Kudos
Reply

1,412 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Tue Jan 12 10:35:33 MST 2010

Quote: mayotte1
If we cut apart the lpcxpresso board, can we plug in the mbed board and used the lpcxpresso debug tools and treat the mbed as just another lpc1768 board?



You can cut apart the LPCXpresso board and use the LPC-LINK section with most LPC1768 development boards such as the RBD1768 from Code Red as long as you stay within the 128KB flash usage limit. In theory one could use the mbed board, but the mbed board does not have the JTAG/SWD signals brought out to the DIP pinout.

http://code-red-tech.com/lpc1768-development-kit.php
0 Kudos
Reply