lpcxpresso_4.2.0_264 version needed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpcxpresso_4.2.0_264 version needed.

1,367 Views
mubashirazhar
Contributor I

Is there a download available for lpcxpresso 4.2.0 version for windows. If yes please provide the link.

I see in downloads page that the last available version is 6.x.x

Thanks

0 Kudos
Reply
2 Replies

1,224 Views
mikesimmonds
Contributor III

I have this archived on my home PC. If you can post a place where I can upload to I can do that for you.

It is approx 208 MB in size. [A little too big for emailing.]

Cheers, Mike.

0 Kudos
Reply

1,224 Views
lpcxpresso_supp
NXP Employee
NXP Employee

That release dates back to 1q 2012 and I'm afraid is no longer available. Projects created with that version ought to load into the latest v8.2.2 version, though I would suggest reading the information in the user guide about updating projects to newer versions of the tools.

Regards,

LPCXpresso Support

0 Kudos
Reply