lpc18xx internal flash settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc18xx internal flash settings

569件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lalitshah233 on Sat Dec 15 21:26:42 MST 2012
Hi all,

I am new to NXP and LPC Xpresso.

I would like to know settings required in LPC xpresso to compile the System to run from internal flash memory of the device.

Also i would like to know how to change this pointer for example i also need to compile the system in such a way that its base address would be

0x1a008000 instead of 0x1a000000

I have tried different settings, have used default settings but could not get success in it.

Regards,
Lalit Shah
0 件の賞賛
返信
1 返信

560件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sun Dec 16 04:21:26 MST 2012
When you create a project for an LPC18xx part with internal flash, such as LPC1857, then an appropriate flash driver will be automatically selected. For more information, please see the FAQ "LPC18xx/43xx Internal Flash Support" at:

http://support.code-red-tech.com/CodeRedWiki/LPC18xx_43xx_InternalFlash

[ Note that you do need to be using LPCXpresso v 4.30 or later to have access to this support.]

Regards,
CodeRedSupport
0 件の賞賛
返信