lpc1769 : ethernet : easy web example not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc1769 : ethernet : easy web example not working

1,550件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sudeep on Mon Jun 25 20:13:29 MST 2012
hello,
  I am trying to communicate with the lpc1769 through the ethernet by running the
example easy web,i have made required connections with RJ45 connector.
when i try to link with http//: ip address:port form another PC the browser is giving error,
is there any thing i have to change in the code  of  easy web project
So if anybody knows how to work on ehternet please reply
0 件の賞賛
返信
5 返答(返信)

1,383件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jun 26 07:17:38 MST 2012

Quote: sudeep


my PC's IP address is 192.168.0.5 and i have burned the same to my lpc board



You are using the same IP address for your PC and target board. You cannot do this - each IP address must be unique within your network.
0 件の賞賛
返信

1,383件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Tue Jun 26 07:07:34 MST 2012
Hi,

It sounds like you are connected to a network. For testing purpose, please make it as simple as possible:
- Connect the board and your PC directly (without any router/switch in between) to each other with a cross-cable.
- Configure your PC to use a static IP address (e.g. 192.168.0.5)
- Configure easyweb to use a static IP address within the same subnet as your computer (e.g. 192.168.0.6).

And try to connect again.

Also have a look at
http://ics.nxp.com/literature/presentations/microcontrollers/pdf/code.bundle.lpc17xx.keil.emac.pdf
for more information on running the easyweb example.

Regards,
0 件の賞賛
返信

1,383件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sudeep on Tue Jun 26 04:58:32 MST 2012
hello sir,

   i am using the same code as in easyweb example given.
    out of  2 red colour leds on the board 1 is blinking with the signal i think this may be the rx line and another line is not blinking its ON only,

the second thing
my PC's IP address is 192.168.0.5 and i have burned the same to my lpc board with the port number as 80.and from the other PC if i try to connect by starting  the firefox  browser and type the link http://192.168.0.5:80 the  fire fox is giving the error as "check your internet connections" that all,according to the example it should
show the web page transmitted by the board

        the third thing  is please explain the produce and consume index concept with example as i have not understood from the  datasheet(user manual).
      
      due to huge code in the example i can't locate from where RXProduce Index is incrementing and it showing 3.

regards
0 件の賞賛
返信

1,383件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Tue Jun 26 00:52:31 MST 2012
Dear sudeep,

What error is the browser giving?
How did you connect your board to your PC and what is the IP configuration of your PC and easyweb?

Regards,
0 件の賞賛
返信

1,383件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by researchinnovation on Mon Jun 25 22:19:32 MST 2012

Quote: sudeep
hello,
  I am trying to communicate with the lpc1769 through the ethernet by running the
example easy web,i have made required connections with RJ45 connector.
when i try to link with http//: ip address:port form another PC the browser is giving error,
is there any thing i have to change in the code  of  easy web project
So if anybody knows how to work on ehternet please reply




Hi...!!!


http://knowledgebase.nxp.com/showthread.php?t=1495
http://knowledgebase.nxp.com/showthread.php?t=2855
http://www.keil.com/forum/16852/
http://forum.flashmagictool.com/index.php?topic=3972.0


Thanks & Regards....:)
0 件の賞賛
返信