lpc13xx RI timer SYSAHBCLKCTRL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc13xx RI timer SYSAHBCLKCTRL

1,431 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuxx on Mon Jan 14 15:29:39 MST 2013
In section 19.2 of the user manual, it says that the RTI clock must be enabled by setting bit 25 of the SYSAHBCLKCTRL register. However in table 19 of the same manual bit 25 is marked as "reserved".

I am confused... is bit 25 the RTI clock enable or is it reserved? There seems to be an error in the manual.

Any help would be appreciated.

Thanks
0 Kudos
Reply
6 Replies

1,411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mcembedded on Thu Jan 17 20:17:55 MST 2013
Hi tuxx,
Yes, bit 25 in SYSAHBCLKCTRL is reserved. RTI is always running so do not need to enable it. We are releasing corrected user's Manual soon.

Thanks,
NXPSupport
0 Kudos
Reply

1,411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jan 15 03:04:04 MST 2013
I always hope someone responsible from NXP is reading our threads here :eek:

But of course you can add a thread to:

http://forums.nxp.com/viewforum.php?f=1

or

http://www.lpcware.com/
0 Kudos
Reply

1,411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuxx on Tue Jan 15 02:30:36 MST 2013

Quote: Zero
Since Chapter 19: LPC1315/16/17/45/46/47 Repetitive Interrupt Timer(RI timer) is a new feature it's SYSAHBCLKCTRL bit has probably been forgotten in Table 19 of User Manual. So I would guess it's disabled by default and you have to enable it as usual in your Init code :)



alright. Should I report the mistake somewhere?
0 Kudos
Reply

1,411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jan 15 01:46:31 MST 2013
Since Chapter 19: LPC1315/16/17/45/46/47 Repetitive Interrupt Timer(RI timer) is a new feature it's SYSAHBCLKCTRL bit has probably been forgotten in Table 19 of User Manual. So I would guess it's disabled by default and you have to enable it as usual in your Init code :)
0 Kudos
Reply

1,411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuxx on Tue Jan 15 01:13:07 MST 2013

Quote: Zero
Disabled ;)

Could be useful if you disclose us which UM you are talking about (something like UM10524 Rev. 2 — 19 November 2012) :)



Yes exactly. UM10524 Rev 2 - 19 November 2012.

What do you mean by "disabled"?
0 Kudos
Reply

1,411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jan 14 16:34:01 MST 2013

Quote: tuxx
I am confused... is bit 25 the RTI clock enable or is it reserved?



Disabled ;)

Could be useful if you disclose us which UM you are talking about (something like UM10524 Rev. 2 — 19 November 2012) :)
0 Kudos
Reply