lpc11xx support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc11xx support?

760件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fentechnt on Mon Dec 14 08:12:22 MST 2009
When will LPCXpresso support the lpc11xx series?  I note that there is now an lpc11xx blinky project available for download from nxp, but it is of little use when the build environment doesn't support the lpc11xx...

I've got a project already started for the 11xx, but may need to decide to move to the lpc13xx instead, if timescales don't fit.
0 件の賞賛
返信
1 返信

752件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Mon Dec 14 11:43:37 MST 2009
An update to LPCXpresso to add LPC11xx support is being tested internally and will be released soon.
0 件の賞賛
返信