lpc-link not found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lpc-link not found

5,044 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andre.marschalek on Fri Jun 19 11:22:32 MST 2015
should LPCXpresso_7.8.0_426 work with windows 10 ?

i have 2 issues, one during installation (error message, screenshot attached) and the second LPCXpresso is not able to find the LPCXpresso Board for LPC11C24
0 项奖励
回复
9 回复数

4,564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jul 01 13:14:45 MST 2015
The standard boot works ok here on latest Windows 10 build (10074). Suspect it is your USB ports. Did you follow all of the troubleshooting in the FAQ?
0 项奖励
回复

4,564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andre.marschalek on Wed Jul 01 08:57:51 MST 2015
thank you

bootLPCXpresso.cmd hid solved that issue

i never had to run that command before, is win 10 the reason?
0 项奖励
回复

4,564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jul 01 08:24:29 MST 2015
Please read this FAQ for troubleshooting booting LPC-Link
http://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link
0 项奖励
回复

4,564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andre.marschalek on Wed Jul 01 08:11:04 MST 2015
ok the error message during installation is gone after system restore was enabled

but

please tell me why lpcxpresso is not able to find my board, its a OM13012 and the board is listed in device manager as USB Device with DFU Capabilities
LPC-Link (HID) not found
0 项奖励
回复

4,564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jul 01 07:28:35 MST 2015
Further investigation has shown that this error is caused if Windows "System Protection" is disabled. System Protection is the Windows service for handling restore points.

It seems that the Windows 10 Build 10074 default setting is for System Protection to be disabled (it is enabled in earlier builds, and in previous versions of Windows).

To resolve this issue on any version of Windows, enable System Protection (use your favorite search engine if you do not know how to do this).

The next version of LPCXpresso will trap the error, report that the System Restore point has not been created, and will continue to install drivers.

0 项奖励
回复

4,564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jun 30 13:28:11 MST 2015
The error message is because the installer is unable to create a system restore point. This implies your are not installing as an administrator ( or perhaps a bug in Windows 10 a which build of Win 10 are you using). Make sure your user has sufficient privileges to create the restore point.

Because of the error, the drivers are not being installed. Therefore you need to install the drivers. Plugin your device and then install the missing drivers, found in the Drivers directory.

The next version of LPCXpresso will continue to install drivers even if a restore point cannot be created.
0 项奖励
回复

4,564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andre.marschalek on Tue Jun 30 11:01:21 MST 2015
i have tried 2 different windows 10 pc's (#10130) one has only usb3 and the other one only usb2 ports
the installation was done with admin rights, one pc was a completely new #10130 installation, the second an update

and both had the same "SWbemObjectEx" error message
0 项奖励
回复

4,564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Jun 19 14:46:25 MST 2015
We had the same message (W10 Build 10130) and Device Manager was showing driver problems...

After Updating the drivers this issue was solved and Link (LPCXpresso11C24-Board) and Link2 are working...
0 项奖励
回复

4,564 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jun 19 13:50:01 MST 2015
We have been testing LPCXpresso on various pre-releases of Windows 10, and have experienced no problems. We will of course support the released version of Windows 10, when available.

The "SWbemObjectEx" problem has been reported on Windows 8 but we have not been able to reproduce. I suspect that it may be due to creating the System Restore point before installing the device drivers. To help us understand if this is the case, are restore points enabled, or does your account have sufficient privileges? I this is not the issue, please run the installer with the /log="install.log" option and post the generated log file.

Regarding the LPC-Link problem: Are you refering the LPC-Link or LPC-Link2? What type of USB port are you connecting to USB2 or USB3? Have you tried another port?

Also, take a look at the Troubleshooting section of this FAQ:
http://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link
0 项奖励
回复