launch failure every other attempt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

launch failure every other attempt

1,079件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sjondur on Tue May 22 16:39:14 MST 2012
Launching usbcdc

1. Program downloads and launches.
2. Press red square, it stops successfully.
3. Press Debug and it hangs at 57% Launching.
4. Press red square, and nothing happens.
5. Press red square a couple of times, few seconds later a window shows up with "Terminate failed."
6. Acknowledge "terminate fail"
7. After ~20 seconds it stops.
8. Press Debug, it reports a license restriction with "Ok" as the sole option.
9. The program is running.

The process from 3. to 8. is about 3 minutes.

This is repeatable.

It seems like I am doing something wrong.
Is there a way to get around steps 3. to 8. and just launch the thing twice in a row?

Thanks.
0 件の賞賛
返信
4 返答(返信)

1,072件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu May 24 05:35:11 MST 2012
I've just tried debugging an LPC1343 mounted on an NGX baseboard here (on a native Win7-32 machine) - no problems seen.

It does sound like it might be a baseboard issue - if nothing else, make sure that you have the LPCXpresso board mounted correctly - there is a picture showing this on the first page of NGX's manual...

http://www.shop.ngxtechnologies.com/download/user_manual/mbed_Xpresso_Baseboard/NGX_Xpresso_1343_mX_...

Another thing to check would be how are you powering the board. I strongly suggest providing additional power to it - the LPCXpresso board is unlikely to be able to provide sufficient power to the baseboard for reliable operation. Another thing to try might be to use an alternative USB port on your computer too.

Finally check the docs and potentially NGX's forums for advice on jumpers etc. Unfortunately we at CodeRed are not currently that familiar with this baseboard, so cannot really provide much advice on its use.

Regards,
CodeRedSupport
0 件の賞賛
返信

1,072件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stalisman on Thu May 24 00:52:38 MST 2012
When my debug has gone all squiffy I just unplug and then replug in the usb connector to the LPC-Link.

If that fails I just restart the IDE.

nothing in this world is perfect :-)
0 件の賞賛
返信

1,072件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sjondur on Wed May 23 12:59:29 MST 2012
Windows XP, osx 10.7 virtualbox.
LPC1343 + mx-base board

The same thing happens with blinky.

If I wait long enough 2-3 minutes, it appears to be running in the IDE but it is not blinking.
LED2 is bistable.
crt_emu_lpc11_13_nxp.exe is still running.
The debug "Console" is clear.

If I suspend it then it says symbol not available in the "Debug" tab.
/No source available for ""/ in the editor.

If I run LPC1343 [I]without[/I] the mx-base board I don't observe this behavior, so it has something to do with the base Board.
0 件の賞賛
返信

1,072件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed May 23 11:15:37 MST 2012
Not something I've ever seen. There isn't really enough information in your report to make an educated guess as to what might be happening though. For example....

What host operating system?

What target board?

After you terminate the first connection, double check that there are no crt_emu_* (exact name depends upon target) still running.

What happens if you leave things for a minute or 2 rather than trying to terminate when the tools are at 57%?

It might be worth booting the board into ISP mode before connecting....

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip

Do you also get the same behaviour if you create a fresh workspace, import a "standard" blink app from the examples, and try downloading that?

Regards,
CodeRedSupport
0 件の賞賛
返信