crp constant doesnt get linked in

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

crp constant doesnt get linked in

746 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Tue Mar 24 11:24:48 MST 2015
I cant seem to get the crp constant to be placed in the linked output. If nothing else I want to at least have 0xFFFFFFFF placed at 0x1FC so I can debug the project.

At first the project wizard included the crp.c and crp.h files, so I moved the source code into main to try and force the issue but after building all I get is...

the source code in main (after moving it to main from crp.c and crp.h)...

#define __CRP __attribute__ ((used,section(".crp")))

#define CRP_NO_CRP          0xFFFFFFFF

__CRP const unsigned int CRP_WORD = CRP_NO_CRP ;

disassembly listing...

int main(void) {

000001fc <__main>:
     1fc:e92d4008 push{r3, lr}
     200:e3a00000 movr0, #0

I am using LPCXpresso v7.6.0 [Build 321] [2015-01-26] on a win 7 machine.
The target device is a lpc2468

Thanks.
Phil
0 项奖励
回复
1 回复

726 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Tue Mar 24 12:01:25 MST 2015
Never mind. I failed to allow crp in the project wizard originally.

All is well.
0 项奖励
回复