bootLPCXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bootLPCXpresso

1,064件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tecnosys on Tue Jun 15 05:48:48 MST 2010
I've installed fresh installation with XP on another machine and installed LPCXpresso 3.3.4 170 . But for some reason the LPCLink/Debug(Cant find emulator) wont work automatically in the IDE. I have to run this command under bin/Scripts to get everything working. Is there a way to fix this? I've tried re-installing the IDE and unistalling the drivers many times. And does'nt seem to help

Jase
0 件の賞賛
返信
3 返答(返信)

1,052件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Jun 16 07:23:38 MST 2010
In that case, can you explain *exactly* what you are doing and all of the error messages you receive. And *exactly* what your are doing that 'fixes' it. I can't see your screen from here ;-)
0 件の賞賛
返信

1,052件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tecnosys on Wed Jun 16 06:16:21 MST 2010
nah, that doesnt help. Any other suggestions
0 件の賞賛
返信

1,052件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 15 06:41:07 MST 2010
Hi,

Can you try changing the following preference:
Window->Preferences
LPCXpresso
  Debug

and check the "Initialise LPC-Link as HID" button.

Unplug and then reconnect LPC-Link and then try again.
0 件の賞賛
返信