blinky troubles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

blinky troubles

1,194 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by raphaelabrams on Mon Nov 04 12:06:07 MST 2013
I'm trying to get some example code to run. I am following the instructions in the getting started guide.

Here's what the "error reported by target" dialog box tells me when I try to debug:

  Flash driver "ProgramPage" timeout (300 ms)  PC: FFFFFFFE
  Flash driver "ProgramPage" timeout (300 ms)  PC: FFFFFFFE
  Flash driver "UnInit" return code: 0x0
  15: Target error from Commit Flash write
  Timed-out programming flash.


It looks like the programmer is trying to go to nonexistent memory?

0 Kudos
Reply
3 Replies

1,181 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by raphaelabrams on Mon Nov 04 12:59:49 MST 2013
Through a process that involved deleting my example folder and reimporting from a zip file, and lots of fist pounding and cursing, I THINK I have success. Blinking is happening. Changed the code a little, debug again, different blinks. Great!

Thanks!





0 Kudos
Reply

1,181 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by raphaelabrams on Mon Nov 04 12:20:52 MST 2013
OSX 10.8.5 on a macbook pro,

direct USB connection to the port labeled "LPC-Link" on a 11U14 lpcxpresso board. It says "rev A" on there as well. 

IDE version 6.1.0
0 Kudos
Reply

1,181 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Nov 04 12:13:42 MST 2013
Any hint which OS, LPCXpresso Version and hardware you are using?
0 Kudos
Reply