Yay C++

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yay C++

813件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by graynomad on Fri Sep 20 06:25:06 MST 2013
From the LCPXpresso page (http://lpcware.com/lpcxpresso) about the latest version of the IDE.


Quote:
The popular Free Edition of LPCXpresso now offers many features previously only available in the premium Red Suite product (including C++ support), and doubles the download limit to 256KB.




Thanks guys, 256k is nice but no C++ was a real stumbling block and a barrier to entry IMO.

______
Rob
0 件の賞賛
返信
1 返信

803件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Mon Sep 23 15:42:49 MST 2013
Yea, C++ is a good deal since there were hacks where one could enable it.
Picked up a Bambino 200 to play with.  This begs C++ and an RTOS on each of the LPC4330 cores.
Thanks NXP/Code Red

0 件の賞賛
返信