Xpresso IDE + Assembler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Xpresso IDE + Assembler

662件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 0xbin4ry on Fri Oct 11 01:53:53 MST 2013
Hi there,

is it possible to debug ASM code in Xpresso IDE? Furthermore, is it possible to get example codes for LPC XPresso 11U14 with the startup files in ASM, rather then in C?

My goal is to debug the startup file (so before the MCU calls main()), possibly in ASM.

I already compiled a simple blinky demo and disassembled the binary to get the ASM code of ResetISR(). However, I want to debug the code to see, whether this corresponds to the ASC version of the startup.c for the Cortex-M0.

Thanks in advance.
0 件の賞賛
返信
1 返信

634件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Oct 11 06:12:56 MST 2013
So why not just set a breakpoint in the startup code and debug it, rather than using assembly code? You can do this manually (open the startup file in the editor and double click on a line), or by changing the default breakpoint from main() to somewhere else:

http://support.code-red-tech.com/CodeRedWiki/InitialBP

[Note that typically the startup file is compiled with optimisation turned on (-Os). You may want to switch this back to no optimisation (-O0). To do this select the file in Project Explorer view, right click and open its properties.]

If you want to use assembler though, then  use the "Search the forums" box (top right of the main forum page) for 'assembly' or "assembler". You will find lots of previous threads on this subject.

Regards,
LPCXpresso Support
0 件の賞賛
返信