Wrong tooltip for typedef struct

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wrong tooltip for typedef struct

1,522件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Wed Jul 08 12:28:40 MST 2015
Weird: There appear some wrong tooltips when hovering the mouse.

As an example in freqmeas.c (LPCOpen 2.08c for LPC1549 with 7.8.0):
Hovering over FREQMSR_SRC_T in line 47: Tooltip for function Chip_INMUX_SetDMATrigger appears.
0 件の賞賛
返信
5 返答(返信)

1,502件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Sun Jul 12 00:36:02 MST 2015
Yes, it's the original example without any changes. I also made a fresh import of the related LPCOpen package into a new workspace without success.
0 件の賞賛
返信

1,502件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat Jul 11 08:56:32 MST 2015
It's the original periph_freqmeas sample...
0 件の賞賛
返信

1,502件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat Jul 11 08:10:41 MST 2015
Please export and post the exact project so we can investigate
0 件の賞賛
返信

1,502件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Sat Jul 11 02:24:56 MST 2015
Unfortunately no change.
And same behaviour on another machine!
0 件の賞賛
返信

1,502件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jul 08 13:51:28 MST 2015
Try refreshing the index. Right click and select index->refresh
0 件の賞賛
返信