Won't set break point

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Won't set break point

ソリューションへジャンプ
4,968件の閲覧回数
jimschimpf
Contributor II

Using an LPV14111 debugging under LPCxpresso.  Could set breakpoints then suddenly all break points appear with a diagonal line through them and nothing happens when they are hit (i.e. cannot stop and debug program).  I do build the debug version and can see the DEBUG env variable in the build lines.  What have I miss set in the LPCxpresso.  

Also under OSX 10.13.3 is crashes randomly (just disappears and have to re-start.)

Thanks for the help.

ラベル(1)
0 件の賞賛
返信
1 解決策
4,590件の閲覧回数
thefallguy
Contributor IV

Have you accidentally disabled breakpoints?

Help - Eclipse Platform 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,590件の閲覧回数
jimschimpf
Contributor II

Yes, that was the problem.  This is the button I pressed by accident.  Thank you very much. Now breakpoint work again.

--jim schiimpf

bad-button.png

0 件の賞賛
返信
4,591件の閲覧回数
thefallguy
Contributor IV

Have you accidentally disabled breakpoints?

Help - Eclipse Platform 

0 件の賞賛
返信
4,590件の閲覧回数
jimschimpf
Contributor II

Just tried to reset the machine LPCXpresso runs on and that made no difference.  Program is built Debug and loads and runs just fine but breakpoints still show diagonal line through them not just a blue dot. And program does not stop.

0 件の賞賛
返信