Windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 10

820 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ronkrem on Sun Aug 09 18:55:59 MST 2015
I just upgraded to W10 and have several problems, one of which concerns LPCXpresso. Compiling a program that was working under W8.1 produces this message:

11:43:53 **** Build of configuration Debug for project E300C_USB ****
make -r all
      0 [main] us 0 init_cheap: VirtualAlloc pointer is null, Win32 error 487
AllocationBase 0x0, BaseAddress 0x71110000, RegionSize 0x4D0000, State 0x10000
C:\nxp\LPCXpresso_7.9.0_455\lpcxpresso\msys\bin\make.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0

11:43:53 Build Finished (took 97ms)

The install of v7.9.0_455 was performed under W10 and seemed to have no problems. Any suggestions welcome.

0 Kudos
Reply
1 Reply

728 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Aug 09 22:59:37 MST 2015
See: https://www.lpcware.com/content/faq/lpcxpresso/virtual-alloc-pointer-null-error
0 Kudos
Reply