Wi Fi Module to use with LPCXpresso 1343

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wi Fi Module to use with LPCXpresso 1343

736 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tomatongo on Thu Jan 27 17:50:35 MST 2011
We are researching a Indoor Location System (Like GPS but inside buildings) and trying to scan available Networks and it's RSSI for pattern matching.

Anyone has done some work with connecting an LPC1343 to a Wi Fi Module? I think we wont be needing TCP/IP Stack (only Phy) so LPC1343 will be enough to do the trick.
Any ideas or suggestions of chips to start working with?


Thanks in advance!!!

Tom.
0 项奖励
回复
1 回复

713 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by oingo456 on Fri Jan 28 10:46:23 MST 2011
Red Pine has some modules that have their own internal TCP/IP stack.  You can just hook them up over a serial port and use some escape codes to set up the wireless channel, etc.  Might be easier.  Data throughput is limited by the serial connection though.
   They also have some that don't have a stack, but the sample drivers might be for windows CE or something.
0 项奖励
回复