Where is my .bin file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is my .bin file?

650 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ECamino on Thu Jan 23 09:07:51 MST 2014
Hi,

I'm trying to create a Release build .bin file.  The post build step is:

arm-none-eabi-size "${BuildArtifactFileName}"; # arm-none-eabi-objcopy -O binary "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin" ; checksum -p ${TargetChip} -d "${BuildArtifactFileBaseName}.bin"; 

When I compile, there are no errors, the build Console says the post build is executed, but then there is no .bin file showing up in the Release directory (or anywhere else on the computer).

Using Windows 7 and LPCXpresso V6.0.2

Thanks,

EC
0 Kudos
Reply
1 Reply

602 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jan 23 09:45:06 MST 2014
In the post-build steps a '#' character is a comment. Everything after a # is ignored.
0 Kudos
Reply