Where is loader's output map file ??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where is loader's output map file ??

776 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Michael.Eaton on Fri Dec 12 09:24:13 MST 2014
Having apparent mem map problem attempting to use LPC4313 on Xpresso v7.5.  The program loads fine into an LPC4337 NGX demo board, but when processor selection is changed to LPC4313 to use on a different board, the debugger reports "no source available for 0x19e80c8c" - no physical memory exists at this loc.

I need to inspect the linker map file to find where it is trying to put the various code blocks.  What is filename for this file, and where is it?

Thank you,
Michael Eaton
0 项奖励
回复
1 回复

760 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Michael.Eaton on Fri Dec 12 10:24:25 MST 2014
Found it - no reply needed.
Thanks,
Mike
0 项奖励
回复