Vector catch and ISP mode doesnt help to get debuger work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vector catch and ISP mode doesnt help to get debuger work

1,203件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zanak on Wed Jun 06 05:05:58 MST 2012
Hello,
I'm still experiencing a strange behavior with the lpcXpresso dev board and IDE.
I was playing with a new lpc11c24 board (from embedded artists) , when I try to debug one of the example projects , I can download succesfuly the file to the flash , but the processor hangs on this line
while (!(LPC_SYSCON->SYSPLLSTAT & 0x01));   
seems like he is unable to get the PLL locked. I tried to get into ISP mode and the vector catch , same problem.
even after erasing the flash with flash magic the process still hangs on the same line.
I tried to create a new workspace then loaded the example projects.
still the same !!
any hint please/
0 件の賞賛
返信
4 返答(返信)

1,189件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zanak on Fri Jun 08 10:58:17 MST 2012
well I'll try to figure out the problem. thank you Zero for your valuable hints.
0 件の賞賛
返信

1,189件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jun 07 13:35:48 MST 2012
With SYSPLLCLKSEL_Val 0x00000000 you've switched to IRC (12MHz, 1% accuracy) as PLL source :)

Probably your timer problem is something different :eek:
0 件の賞賛
返信

1,189件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zanak on Thu Jun 07 13:11:41 MST 2012

Quote: Zero
If your PLL isn't running, ISP or vector catch doesn't  help. Either your code is faulty or your PLL source (crystal?) is  damaged :eek:


thank you Zero .
I think my crystal is damaged ! I switcher to the  IRC and now I'm able to get over the wait condition. but I still don't  understand how my crystal can be damaged !

I changed #define  SYSPLLCLKSEL_Val   to   0x00000000. do I need to modify other defines to  get the system work correctly. cause the timer is running too fast  which make me think that I still miss something in the config file.
thanks in advance
0 件の賞賛
返信

1,189件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Jun 06 05:22:41 MST 2012
If your PLL isn't running, ISP or vector catch doesn't help. Either your code is faulty or your PLL source (crystal?) is damaged :eek:

You could try to start your LPC without PLL in IRC :)
0 件の賞賛
返信