VCOM port .inf file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VCOM port .inf file

1,311 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by inspire on Tue Apr 07 12:12:46 MST 2015
Hi,

in the LPC43xx LPCopen package there is a usbd_rom_cdc_vcom example. But when I flash the software to my NGX board, Windows 7 can't find any drivers for the VCOM. Also, in the project readme it says "When connected to Windows host use the .inf included in the project directory to install the driver."

But there is no such .inf file in the project directory.

Where can I find it?

Thanks!
Martin
0 Kudos
Reply
2 Replies

1,167 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by inspire on Fri Apr 10 10:17:58 MST 2015
Ah great, thanks for your help!
0 Kudos
Reply

1,167 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Apr 07 17:36:00 MST 2015
Hi Martin,
Second last column of below page points to driver
http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc43xx-packages

You can also try inf from
http://www.lpcware.com/system/files/lpc43xx-vcom.zip
0 Kudos
Reply