Using the lpc3154 for other duties

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the lpc3154 for other duties

1,018件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Kartman on Fri May 06 04:16:04 MST 2011
Please excuse me if this has been asked before, with the lpc3154 on the Lpc-link, can we download our own code using dfu or other modes? Reading the datasheet suggests that the code can be encrypted and the key stored in one time programmable memory, so this might prevent other code from being loaded. If we can load code, can we use one lpc- link to debug another (with the required wiring)?
0 件の賞賛
返信
2 返答(返信)

1,004件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Kartman on Fri May 06 05:47:14 MST 2011
Thanx zero, once again. It all comes down to the words one searches on! The answer was what I expected, but didn't want to hear.
0 件の賞賛
返信

1,004件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri May 06 04:36:16 MST 2011
Wasn't that answered by NXP_USA?

http://knowledgebase.nxp.com/showthread.php?p=36
0 件の賞賛
返信