Using the lpc3154 for other duties

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the lpc3154 for other duties

1,015 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Kartman on Fri May 06 04:16:04 MST 2011
Please excuse me if this has been asked before, with the lpc3154 on the Lpc-link, can we download our own code using dfu or other modes? Reading the datasheet suggests that the code can be encrypted and the key stored in one time programmable memory, so this might prevent other code from being loaded. If we can load code, can we use one lpc- link to debug another (with the required wiring)?
0 Kudos
Reply
2 Replies

1,001 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Kartman on Fri May 06 05:47:14 MST 2011
Thanx zero, once again. It all comes down to the words one searches on! The answer was what I expected, but didn't want to hear.
0 Kudos
Reply

1,001 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri May 06 04:36:16 MST 2011
Wasn't that answered by NXP_USA?

http://knowledgebase.nxp.com/showthread.php?p=36
0 Kudos
Reply