Using USB ram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using USB ram

785件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kemes on Tue Apr 09 22:10:26 MST 2013
Hi to all
I am using LPC11U37 with  LPCXpresso v5.1.2 [Build 2065] [2013-02-20].  Due to the fact that some RAM is reserved to USB, there is a way to force assigning a buffer to USB RAM ?  I saw that I should enable the clock setting USBRAM bit in SYSAHBCLKCTRL.
How can I force some data to be allocated in this ram ?
thanks
0 件の賞賛
返信
1 返信

714件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by daniel.widyanto on Tue Apr 16 19:54:24 MST 2013
Modify your linker file. Refer to http://support.code-red-tech.com/CodeRedWiki/EnhancedManagedLinkScripts
0 件の賞賛
返信