Using Red Probe+ to program HEX file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using Red Probe+ to program HEX file

975 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Petervg on Tue Jun 12 05:32:05 MST 2012
Hi,

I have an older design where I don't have the source code, but I need to program the LPC2214 with an HEX file.

Is this possible using the red probe +? In LPCXpresso I can't find any options to flash a hexfile into a controller...

With kind regards
Peter
0 Kudos
Reply
2 Replies

965 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jun 12 06:06:09 MST 2012
Safest way is to use FlashMagic :eek:

It's able to flash 2214 and it cares about your checksum (if necessary) :)
0 Kudos
Reply

965 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jun 12 06:00:39 MST 2012
AFAIK, LPCXpresso can only program bin and axf (elf) files. There are lots of hex to binary file converters available.
0 Kudos
Reply