Using LPC1114 driver files for LPC11A14

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using LPC1114 driver files for LPC11A14

966 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shashankiim on Tue Mar 05 20:09:54 MST 2013
Hi Guys

I have a quick question. I was having LPC1114FBD48(48 pin)  lpcxpresso development board which I used for development. Now I want to use LPC11A14FHN33(33 pin) in my final design.

Can I use the driver files and examples programmes of LPC1114 for LPC11A14 ?
As I go through there are a lot of example projects for LPC1114 but no example projects for LPC11A14 in LPCxpresso.

For example can I make a project for LPC11A14 and import "uart.c/h" and "i2c.c/h" driver files from the example codes of LPC1114 and use them for LPC11A14?

Any pointers will be really helpful.

Rgds
Shashank
0 Kudos
Reply
1 Reply

877 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Wed Mar 06 00:46:54 MST 2013
Try NXP's LPC11Axx software example page at:

http://www.lpcware.com/gfiles/all?tid_1%5B%5D=157&tid_2%5B%5D=8

HTH!
0 Kudos
Reply