Using ITM on LPC13xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using ITM on LPC13xx

1,719件の閲覧回数
prachipanse
Contributor III

Hi,

The LPCXpresso IDE Instruction Trace Guide states that the instruction trace is not supported on the LPC13xx devices. However, as per the device datasheet, it seems like it may be supported -"Instrumentation Trace Macrocell allows additional software controlled trace." is mentioned as a feature of SWD.

Can you please confirm is it is supported by this chip?

Regards,

Prachi

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,569件の閲覧回数
prachipanse
Contributor III

Thanks. I now understand that LPC13xx does not support Instruction Trace since ETM or ETB are not implemented. However, ITM can be used if the SWO pin is connected.   

0 件の賞賛
返信

1,569件の閲覧回数
thefallguy
Contributor IV

Don't get confused between Instruction Trace and Instrumentation Trace Macrocell (ITM). . As it says in the manual

  • Note that instruction trace is not supported with LPC17xx MCUs (which do not implement an ETB) or LPC13xx/LPC15xx MCUs (which do not implement ETM or ETB).

ITM does not support Instruction Trace, for that you need the additional hardware in the processor core - ETM/ETB or MTB.

0 件の賞賛
返信