Use mbed as target board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use mbed as target board?

1,235件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hansi on Sat Jul 12 08:19:28 MST 2014
Hi!

For a little project I wanted to use the LPCXpresso Board for the LPC11U24 (OM13066). After searching through my eval boards I found out, that I "only" have an mbed-LPC11U24 but not the larger LPCXpresso board.

My question is now: Can I use this little mbed board together with the LPCXpresso 7.2.0 IDE?

I'm aware that I could simply copy the compiled executable file to the simulated USB stick. But can I use the LPCXpresso to connect via USB and further JTAG/SWD, i.e. do debugging? Do I need any extra hardware or is it enough to plug in the USB cable?

Thanks
  Hansi
0 件の賞賛
返信
5 返答(返信)

1,201件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jul 23 06:12:00 MST 2014
Assuming that you are using LPCXpresso 7, you don't need to do anything in LPCXpresso to recognise a CMSIS-DAP probe. Just connect it to your PC and start debugging and it will be found. If your debug session previously used a different debug probe, you will be shown an empty list of debug probes and you can "Search Again"
0 件の賞賛
返信

1,201件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hansi on Wed Jul 23 06:04:15 MST 2014
Thanks for the hint!

Could you please explain how to setup thie CMSIS-DAP probe in LPCXpresso? I didn't find it on the referenced URLs, nor in any settings dialogs.

Thanks
  Hansi
0 件の賞賛
返信

1,201件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jul 14 04:21:32 MST 2014
I haven't actually tried an LPC11U24 mbed board - but on the assumption it provides a CMSIS-DAP debug interface, then yes - you should be able to connect to this from the LPCXpresso IDE. Note that you may need to the latest firmware..
http://mbed.org/handbook/Firmware-LPC1768-LPC11U24

For more information on CMSIS-DAP support in the LPCXpresso IDE, see:

http://www.lpcware.com/content/faq/lpcxpresso/cmsis-dap-support

Also note that you will also need the mbed Windows USB serial drivers installed.


Regards,
LPCXpresso Support




0 件の賞賛
返信

1,201件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hansi on Sat Jul 12 09:38:33 MST 2014
Thanks for your answer.

I'm aware that I can use the LPCXpresso Boards as JTAG/SWD "driver" and already did that with several custom LPC11U14 PCB projects.

My question is: does LPCXpresso support the mbed LPC11U24 PCB out of the box and without hardware modifications as a target board for JTAG/SWD access?

Thanks
  Hansi
0 件の賞賛
返信

1,201件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Sat Jul 12 09:09:09 MST 2014

Quote: Hansi
My question is now: Can I use this little mbed board together with the LPCXpresso 7.2.0 IDE?



Yes, we can  :)

To use LPCXpresso (Flashing / Debugging) you need a Link / Link-2 and SWD connection to your board.

I'm not familiar with this mbed board and don't know if  there's a connector to access SWDIO, SWCLK and Reset.

Anyway, it's a LPC11xx and this 3 signals are enough to use SWD / LPCXpresso...

Probably this signals are connected to the MBED chip also, so you should disconnect them there...

Overall I wouldn't recommend to do that. An OM13066  isn't so expensive and you don't risk to ruin your mbed board...
0 件の賞賛
返信