Updated to version 8, now cant debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Updated to version 8, now cant debug

1,011 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TVinto on Tue Dec 15 09:35:41 MST 2015
Hi,

I have an LPC1837-Xplorer board and I am using that for the following...

I had version 7 running OK. ( have not used it in a couple of months )
I uninstalled 7 and then downloaded and installed the latest version 8 LPCExpresso yesterday.

I created a new workspace and imported all LPCOpen projects for "NXP LPC1837/LPC18S37 LPCXpresso board".  I downloaded a fresh copy yesterday too.


I built all and that went OK

I selected the periph_blinkey project and pressed the debug link in the quickstart panel.

That build OK but when it tries to load the CMSIS-DAP it times out.  ( sorry I dont have the exact dialog but my LPCExpresso is frozen and I dont want to re-boot just yet )

It offered to show a log file, but that looks more like a dump of random text ...like the program blew up.

I press "abort" when prompted.

LPCxpresso is frozen after that.



Not sure how to proceed.  Could there be something left behind from version 7 that needs to be cleaned up? ( I ran the uninstall.exe and then deleted the version 7 directory )

please help...
Thanks, Vint
0 Kudos
Reply
3 Replies

1,004 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TVinto on Tue Dec 15 11:55:42 MST 2015
Thanks!
Your link on failing enumeration did it.
My LPCLink II driver was the 1.0.0.0 revision.





0 Kudos
Reply

1,004 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Dec 15 10:13:10 MST 2015
Depending on your host OS, if it is a version of Windows and you have moved from a slightly older version of LPCXpresso IDE, then the most likely cause if you are using an LPC-Link2 debug probe is the driver issue for the CMSIS-DAP debug probe firmware that we now use...

https://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-failing-enumerate-cmsis-dap-firmware

PS : If moving from an older version - you might also want to read:

https://www.lpcware.com/content/faq/lpcxpresso/migrating-new-version-LPCXpressoIDE

In particular, there is generally no need to uninstall the old version when you first install the new one.

Regards,
LPCXpresso Support
0 Kudos
Reply

1,004 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Tue Dec 15 09:54:50 MST 2015
Did you read this?
https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link2

Read the troubleshooting section, at the end...
0 Kudos
Reply