Unknown Part Number

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unknown Part Number

1,312件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stalisman on Thu Jul 26 01:30:06 MST 2012
Hi folks,

I have the following error with an LPC1113/301 chip

[SIZE=2][COLOR=#008000][SIZE=2][COLOR=#008000][LEFT]Invalid LPC1113/301 Part ID: 0x2532102B
Known LPC1113/301 ID(s): 0x0434102B[/LEFT]
[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][COLOR=#ff0000][SIZE=2][COLOR=#ff0000]03: Failed on chip setup: Ec(01). Invalid, mismatched, or unknown part

[COLOR=black]Is anything known about this?[/COLOR]
[COLOR=#000000][/COLOR]
[COLOR=#000000]Is it possible that it's a new number and my IDE is out of sync perhaps?[/COLOR]
[COLOR=#000000][/COLOR]
[COLOR=#000000]Is it a part ID for someo other chip that got misscoded?[/COLOR]
[COLOR=#000000][/COLOR]
[COLOR=#000000]etc.[/COLOR]
[COLOR=#000000][/COLOR]
[COLOR=#000000][/COLOR]
[/COLOR][/SIZE][/COLOR][/SIZE]
0 件の賞賛
返信
4 返答(返信)

1,302件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stalisman on Mon Jul 30 03:53:39 MST 2012
I would if I could but I don't have it any more. The good news is though that I binned the chip and got another one fitted that works just fine. I had noticed that it reported an ID of 0x00000000 at one stage and that I thought indicated a damaged chip hence the change.

Cheers
0 件の賞賛
返信

1,302件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Jul 30 00:34:10 MST 2012
[FONT=Courier New][SIZE=2]0x2532102B[/SIZE][/FONT] should be a recognised part ID for LPC1113/301 in LPCXpresso 4.2.3

Please can you post your full debug log from a failed connection...

http://support.code-red-tech.com/CodeRedWiki/DebugLog

Regards,
CodeRedSupport
0 件の賞賛
返信

1,302件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stalisman on Fri Jul 27 03:44:40 MST 2012
[SIZE=2][LEFT]LPCXpresso: [/LEFT]
Version: LPCXpresso v4.2.3 [Build 292] [30/05/2012]

cheers!
[/SIZE]
0 件の賞賛
返信

1,302件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Jul 26 02:19:00 MST 2012
Which version of LPCXpresso are you running?
0 件の賞賛
返信