Uninstall older version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uninstall older version

967 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Thu Dec 04 15:09:43 MST 2014
Hi, I am just getting started with the tool so I have some stupid quesions.


I am trying to uninstall revision 7.3.x  on my Windows 7...

I had revision 7.3 something installed and wanted to update to the 7.5.0.  Could not find any update help so I assumed I could just install the new one.

I ended up with two versions.  I used uninstall in the control panel and it seemed to work.  The 7.5.0 was gone.

However there seems to be no way to uninstall the 7.3 revision.


How do I do that?

Thanks
0 Kudos
Reply
2 Replies

941 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Fri Dec 05 06:35:06 MST 2014
Thanks!
0 Kudos
Reply

941 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu Dec 04 15:35:45 MST 2014
Run the uninstall.exe app in the install directory. It's also on the start menu...
0 Kudos
Reply