Unable to Connect to LPC-Link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to Connect to LPC-Link

752 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by richas on Tue Feb 16 18:21:31 MST 2010
If, I disconnect the LPC-Link while the LPCxpresso IDE is open I cannot ever connect to the debugger again.  I have to restart the computer! (winxp)

I have:
reinstalled LPCxpresso
uninstalled/reinstalled the device under device manager

If I close the IDE and THEN disconnect/reconnect the debugger then, after restarting the IDE I can still connect.

I am doing this to reset the board so I can run code without starting the debugger.

Has anyone else experienced this?

Rich

Original Attachment has been moved to: 1100124_extra%20info.txt.zip

Original Attachment has been moved to: 1100124_extra%20info.txt.zip

Original Attachment has been moved to: 1100124_extra%20info.txt.zip

Original Attachment has been moved to: 1100124_extra%20info.txt.zip

Original Attachment has been moved to: 1100124_extra%20info.txt.zip

Original Attachment has been moved to: 1100124_extra%20info.txt.zip

0 Kudos
Reply
1 Reply

699 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Feb 17 00:24:34 MST 2010
The problem with "pulling the plug" so to speak, is you have effectively stranded (left running) two processes used by the LPCXpresso IDE to communicate with the target. This may hamper your ability to restart the IDE. You can disconnect the debugger, and leave the board executing. Please review:

http://knowledgebase.nxp.com/showthread.php?t=100

Regards,

CodeRedSupport
0 Kudos
Reply