Uartdma

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uartdma

474 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ArunPrasad on Tue Nov 27 02:37:28 MST 2012
I have some problems using UART-DMA. I am communicating two boards by PC through the same RS485 line.
1) In this case can I vary the number of bytes while transmitting and receiving? If so please exlpain how it can be done.
2) DMA is disabled after an interrupt. can we use DMA without re-enabling it everytime like UART interrupt which automatically interrupts the controller when one byte is received..?
0 Kudos
Reply
0 Replies