Uart temp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Uart temp

858件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mohsin on Wed Nov 17 03:52:45 MST 2010
Hi All,

             I am using LPC1114 in my project. I am using uisng UART for driving RS485 and I am controlling the Transmit enable in software.

1) I want to know how could we make use of the TEMP (Transmitter Empty)  flag. All my transmission/reception is interrupt based. As there is no interrupt for TEMP, I need to know when the Transmitter is empty (both U0THR and U0TSR are empty) so that I can disable the Transmit enable.

2) Is there a way to control so that interrupts are based only on TEMP (not on THRE).

3) Is there a way to check if there is space in the Transmit Buffer so that more characters can be written ?
            Regards,
            Mohsin
0 件の賞賛
返信
1 返信

846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gbm on Wed Nov 17 04:14:21 MST 2010

Quote: mohsin
Hi All,
I am using LPC1114 in my project. I am using uisng UART for driving RS485 and I am controlling the Transmit enable in software.


Why not in hardware? Look at RS485CTRL and RS485DLY registers.


Quote: mohsin
2) Is there a way to control so that interrupts are based only on TEMP (not on THRE).


AFAIK, not in this particular UART implementation.


Quote: mohsin
3) Is there a way to check if there is space in the Transmit Buffer so that more characters can be written ?
            Regards,
            Mohsin


THRE == 1 means that there is a place in Tx FIFO. In the interrupt routine write bytes to THR until THRE becomes 0.
0 件の賞賛
返信