USB_VBUS and ADC0_IN[4] - LPC178x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB_VBUS and ADC0_IN[4] - LPC178x

493件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by graynomad on Wed Sep 14 08:10:56 MST 2011
I'm designing a board based on the LPC178x, I need USB and all ADC inputs but there seems to be a clash between USB_VBUS and ADC0_IN[4] and neither can be moved to another pin.

Searching the web I cannot get a definitive answer as whether there is a work around or indeed if VBUS is really needed.

The manual says


Quote:
USB_VBUS — Monitors the presence of USB bus power.
This signal must be HIGH for USB reset to occur.



Does this mean that once the chip (and USB) is booted I can use that pin for my ADC?

I can't believe they would assign two important functions to the pin.

______
Rob
0 件の賞賛
返信
0 返答(返信)