UIP & DNS client problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UIP & DNS client problem

765 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nav1980 on Tue Jun 24 20:09:15 MST 2014
Hi,
I've using the uIP stack to send HTTP posts to a remote webserver with some sensor data. I'm using resolv.c (included as part of uIP) as the DNS client to resolve the remote webserver domain name to IP address. All works well as long as I use the router (192.168.1.1) as the DNS server address. But if I try to use any external DNS server address (such as Google's public DNS server 8.8.8.8), then it fails to resolve. The router firewall is ruled out as I've tried using same external DNS servers on computers whose network settings are manually configured and it works just fine. I'm struck at this problems since a long time and would be grateful if someone can help me solve this problem!

My platform uses the RDB1768 + LPCxpresso. Please let me know if you need any further information.
0 Kudos
Reply
1 Reply

741 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nav1980 on Wed Jun 25 22:01:36 MST 2014
Bumping this up.
0 Kudos
Reply