UART signals?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART signals?

967件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ECamino on Thu Aug 01 06:51:32 MST 2013
Hi,

In one of our applications, we have to drive an optoisolator input with the UART.  Is there a way to invert the TX/RX signals from the UART (LPC1347)?

Thanks,

EC
0 件の賞賛
返信
3 返答(返信)

935件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ECamino on Fri Aug 02 06:03:06 MST 2013
Thanks guys.  We are driving through a cable and did not make provisions to power the anode through the cable and drive the buffer on the cathode to sink and invert the signal...I guess we'll have to make a revision to provide for 5V at the anode on the external opto.

EC
0 件の賞賛
返信

935件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by graynomad on Fri Aug 02 01:01:19 MST 2013
As John says, just wire the opto correctly, either the way you drive the LED or the way you pull the output. Either way can be used to invert the signal.

______
Rob
0 件の賞賛
返信

935件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by js-nxp on Thu Aug 01 15:09:54 MST 2013
If you wire the optoisolator correctly there is no need to invert the signals.

edit why is my signature appearing twice??

2nd edit WOW things are moving fast, the whole interface seems to have now changed.
0 件の賞賛
返信