Two version of installation completing dialogues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Two version of installation completing dialogues

809 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by noritan_org on Sun Jan 31 19:11:31 MST 2010
I have tried to install LPCXpresso IDE many times, and found that there are two version of installation completing dialogues as the last window of the installation wizard.  The dialogue is titled as "Completing the LPCXpresso Setup Wizard" with a "Finish" button.  But there are two versions having contents as follows.

(1) "To complete the installation of LPCXpresso, Setup must restart your computer. Would you like to restart now ?"

(2) "Setup has finished installing LPCXpresso on your computer. The application may be launched by selecting the installed icons."

(1) requires RESTART and (2) does not.  In addition, they have different CheckBoxes and RadioButtons.

My question is :

Q: What is the condition to require a RESTART ?

I must close all other windows prior to a RESTART, but I cannot find the condition if a RESTART required.

Thanks in advance.
0 项奖励
回复
2 回复数

803 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Feb 01 03:31:43 MST 2010
A restart is required if the installer was unable to install a file because it was in use. Any such files are automatically installed on the restart of Windows
0 项奖励
回复

803 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Feb 01 00:41:16 MST 2010
A restart is required if the installer was unable to install a file becuase it was in use.
0 项奖励
回复