Touch Screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Touch Screen

1,132 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cesimkaol on Mon Nov 28 08:43:38 MST 2011
Dear Developers,

I want to attach to touch screen to my project , there will be simple buttons gui, but ı dont have any idea about it..How to develop , which processor of NXP would you recommend me and what about linux ,how to use linux here....
0 Kudos
Reply
3 Replies

1,094 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Tue Nov 29 05:24:46 MST 2011

Quote: cesimkaol
Dear Developers,

I want to attach to touch screen to my project , there will be simple buttons gui, but ı dont have any idea about it..How to develop , which processor of NXP would you recommend me and what about linux ,how to use linux here....



Hi,

Have a look into the following link,
http://www.nxp.com/products/microcontrollers/cortex_m3/lpc1700/LPC1788FET208.html
may it help you for your MCU selection and touch screen interface.

Kind Regards,
0 Kudos
Reply

1,094 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Nov 28 10:21:00 MST 2011
There are a lot of touchscreens available :)

A simple solution is an SPI controlled LCD with SPI controlled touchscreen. That's doable with a simple LPC11C14 and enough for a simple small GUI.

See: http://www.watterott.com/en/MI0283QT-2-Adapter

If you expect more power, use something like LPC1788, especially this kit:

http://www.embeddedartists.com/products/kits/lpc1788_kit.php

That's a very powerful kit and able to use free Segger emWin :cool:

You can use it with a huge 7" :eek: touchscreen as shown here at TechCon 2011:

http://www.youtube.com/watch?v=5mCoQKhtndQ&feature=related

or

http://www.youtube.com/watch?v=IN55_8z7m90&feature=player_embedded
0 Kudos
Reply

1,094 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Mon Nov 28 10:02:15 MST 2011
[B]Touch screen ... [/B]
Select an LCD display that comes with a touch screen controller, or use something like a TSC2046, that one is being used by Embedded Artists on a lot (if not all) of their boards.

[B]Linux[/B]

The LPCXpresso controllers that are being discussed in this forum are too small for Linux. If you want Linux I'd use one of the larger processors (lpc2478 or so).
Embedded Artists still have the lpc2468 Developer's kit (for uClinux) but there are also the LPC3141 board and the LPC3250 Developer's kit that runs 'real' Linux or if you are brave enough to create your own base board use the LPC3250 DIMM module.

But of course it all depends what you want to do.

Rob
0 Kudos
Reply