Hi Support Team,
I followed your instruction above. Below you find the debug output.
However I did some more tests to make sure everything on my Hardware setup is correct.
I connected my LPC-Link 2 linked to the OM27462CDK Board to a "real" Windows machine.
I could start debugging without any problems.
On two of my VM's I connected a LPCXpresso1769/CD OM13085 board.
Also no problems with this board.
Here is the debug Log:
LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:12:38 - crt_emu_cm_redlink build 725)
============= SCRIPT: PN7xxxxx_Connect.scp =============
Hardware interface transfer error
Wire not connected
Wire not connected
Wire not connected
============= END SCRIPT ===============================
Probe Firmware: LPC-LINK2 CMSIS-DAP V5.173 (NXP Semiconductors)
Serial Number: JQD4BWMV
VID:PID: 1FC9:0090
USB Path: \\?\hid#vid_1fc9&pid_0090&mi_00#8&e8b5b46&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
connection failed - Ee(36). Could not connect to core. - retrying
Failed on connect: Ee(36). Could not connect to core.
Connected&Reset. Was: NotConnected. DpID: 00620034. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 0
No debug bus (MemAp) selected
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
(100) Target Connection Failed
While i was trying different things I finally got it working.
The solution is to connect the LPC-Link2 manually to the virtual machine after the booting (DFU) mechanism.
You have to wait for a couple of seconds after the USB device chances to "NXP Semiductor LPC-LINK2 CMSIS-DAP V5.173. If you connect immediately you every time end up with the Error above.
Thank you very much for your assistance.