Software for ISP via CAN LPC11C14

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software for ISP via CAN LPC11C14

1,568 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IGW on Thu Sep 30 22:19:32 MST 2010
Hello all,

Does anyone know of any software that could either:
1) In System Program an LPC11C14 via a CAN bus
  or
2) Source code and documentation to provide guidance on what CAN messages to send and how to format (if necessary) the image for download to the CAN ISP?  I would then write one and it would probably become open source and available for others.

I have seen http://www.flashmagictool.com/ (no CAN), and http://sourceforge.net/projects/lpc21isp/ (different series of processors - but maybe there are some gems there that would provide guidance for the LPC11C1x devices).

Thanks,
Ian
0 Kudos
Reply
2 Replies

1,524 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Jesse.Rosenberg on Fri Oct 01 12:56:00 MST 2010
Flash Magic (www.flashmagictool.com) does. See attached screen shot. From their change logs:
Version 5.66 ------------  - Added support for PEAK PC Card interface.  - Improved user interface for CAN and Ethernet devices.  - Added LPC11C12 and LPC11C14 with UART bootloader.  - Added EM773 and MPT612.
0 Kudos
Reply

1,524 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by igorsk on Fri Oct 01 04:48:27 MST 2010
See the User Manual, Chapter 19.6.
0 Kudos
Reply