Simple question about peripheral labels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simple question about peripheral labels

821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jbrydon on Sun Nov 23 22:45:39 MST 2014
Am new to these devices but not to MPU programming.

I have looked and looked but they have evaded me.

Where are the sets of standard labels defining the peripheral registers, timers and ports, e.g. "LPC_GPIO2" and "SysTick_Handler" etc.

Also, do higher level APIs exist as in mBed ?

JB
0 Kudos
Reply
2 Replies

813 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jbrydon on Mon Nov 24 22:20:28 MST 2014
Thanks that's helpful. However, I'm still seeing the chunks of data I need all over the place.

What I want to do is go, say, to the LPCXpresso LPC1769 schematic, identify which pins I want to use and write code which, say, toggles a particular pin or sets up a particular timer to interrupt on timeout. The information that I need in order to progress through this sequence still seems scattered about.

I haven't, for example, found a document which says, these are the peripheral registers specifically on, for example, the LPC1769 and here are their LPCOpen labels.
0 Kudos
Reply

813 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Nov 24 00:09:37 MST 2014
You need LPCOpen:
http://www.lpcware.com/lpcopen

Examples of which are included  in the "LPCOpen" directory of the installation. Suggest you read the User Manual for instructions on how to use the Example projects.
0 Kudos
Reply