Setup linker parameters manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setup linker parameters manual

956件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MrBool on Wed Mar 18 09:16:55 MST 2015
How can I setup flash size and location? In "MCU settings" memory details are not editable.
For example I use LPC1114FBD48 (32kB flash) and I have in first sector bootloader and last sector I use for store config (iap), so flash location for application should be 0x1000 and size 0x6000.
0 件の賞賛
返信
2 返答(返信)

948件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MrBool on Wed Mar 18 09:59:55 MST 2015
I use the last version. Now I see "Edit.." button. My problem disappeared. Thank you!
0 件の賞賛
返信

948件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Mar 18 09:28:39 MST 2015

Quote: MrBool
In "MCU settings" memory details are not editable.



:quest:

Which version are you using?
0 件の賞賛
返信