Serial Wire Debug: Rising edge or falling edge?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial Wire Debug: Rising edge or falling edge?

589 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JUM on Thu Jul 28 06:48:45 MST 2011
Hi,
according to Figures 5-1 and 5-2 in "ARM® Debug Interface v5 Architecture Specification" the data bits on SWDIO are valid at the falling edge of SWCLK.
BUT: According to Figures 24 and 25 in "ARM® Debug Interface v5 Architecture Specification ADIv5.1 Supplement" the data bits on SWDIO are valid at the rising edge of SWCLK!?
What is true?
Best regards
JUM
0 Kudos
Reply
0 Replies