Segger EMWIN/4088 Compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Segger EMWIN/4088 Compatibility

733 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by paul.rcom-software.com on Thu Jul 24 14:28:46 MST 2014
I am using an Embedded Artists LPC4088-32 dev. board with the Rowley Crossworks toolchain and
LPCXpresso.  Does anybody know if the EMWIN graphics package has been successfully ported
to this environment--or a close one ?

This is the information about the graphics hardware I plan to use.

* On-Board LCD Controller

LCD controller, supporting both Super-Twisted Nematic (STN) and Thin-Film
Transistor (TFT) displays.

- Dedicated DMA controller.

- Selectable display resolution (up to 1024 × 768 pixels)

Selectable display resolution (up to 1024 × 768 pixels)

Features and capabilities are detailed in chapter 11 of the NXP  UM10562 LPC407X/408X User Manual.

NOTES: To be used in conjuction with a Kyocera 3 1/2" QVGA LCD display--model
number T-55343GD035JU-LW-ADN

Best Regards,

Paul R.
0 Kudos
Reply
1 Reply

712 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 25 00:04:05 MST 2014
Please delete this duplicate thread - see http://www.lpcware.com/content/forum/lpc4088-segger-emwin-compatibility for a response
0 Kudos
Reply