Security problem with CRP3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Security problem with CRP3

847件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Fri Jun 24 04:52:51 MST 2011
[FONT=Arial][SIZE=4][COLOR=black]In reading the manual for the LPC111X chips I came accross table 216; "Code Read Protection hardware/software interaction".[/COLOR][/SIZE][/FONT]
[FONT=Arial][SIZE=4][COLOR=black]If I read this properly, the chip will enter ISP mode if the "user code valid" test fails even with CRP3.[/COLOR][/SIZE][/FONT]

[FONT=Arial][SIZE=4][COLOR=black]Thus, if an someone can force the user code valid test to fail then they can read out the code even if CRP3 has been set.[/COLOR][/SIZE][/FONT]

[FONT=Arial][SIZE=4][COLOR=black]One possible way to cause a error in the first 8 vector table entries and thereby cause the chip to enter ISP mode it to raise the temperature high enough to cause the bits in the flash to fail. After scanning out a few chips and correcting for the errors you could get a good image of the code even if CRP3 is set.[/COLOR][/SIZE][/FONT]

[FONT=Arial][SIZE=4][COLOR=black]I understand that the same technique could be used to attack the CRP3 value directly but the "valid user code" makes the attack easier.[/COLOR][/SIZE][/FONT]

[FONT=Arial][SIZE=4][COLOR=black]Is this realistic or am I just being paranoid?[/COLOR][/SIZE][/FONT]

[FONT=Arial][SIZE=4][COLOR=black]Pete.[/COLOR][/SIZE][/FONT]
0 件の賞賛
返信
1 返信

816件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by igorsk on Fri Jun 24 07:22:02 MST 2011
Another common technique is voltage glitching. If you want real security, get a security hardened processor with encrypted code storage. CRP is not a real barrier for determined people.
0 件の賞賛
返信