Rx Interrupt driven SSP bus master

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rx Interrupt driven SSP bus master

475件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JSalisbury on Tue Apr 12 03:14:13 MST 2011
Hi,
I am using an LPC1114 and wanting to use a SSP bus master to obtain 24 bits in two 12 bit transactions, at 32KHz intervals. The master clock will be about 48MHz I will be setting the busmaster to set SSP clock to 5MHz. Is it possiable to use an interupt to service this, or would the serviceing of the interupt take a significant part of 2.4us and so not worth it?

Thanks
0 件の賞賛
返信
0 返答(返信)