Request for sample code of LPC17xx VCOM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for sample code of LPC17xx VCOM

1,101件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by raymond.centek on Thu Jan 12 04:01:12 MST 2012
Is there any Virtual COM (VCOM) sample code for LPC17xx Expresso Board using nxpUSBlib? Thanks
0 件の賞賛
返信
3 返答(返信)

1,055件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by raymond.centek on Fri Jan 13 20:10:27 MST 2012
Thank you for the replies.
I want to use VCOM because I want to implement the communication between LPC1769 and android tablet. I tried AOA and the speed is not fast enough. However, the AOA seems can be speed up by changing the config. I will ask this at another thread.
0 件の賞賛
返信

1,055件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Thu Jan 12 18:18:01 MST 2012
We are working on an nxpUSBLIB VCOM example and should have something finished within the next couple of weeks.
0 件の賞賛
返信

1,055件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gbm on Thu Jan 12 13:04:05 MST 2012
Yes, there are at least 3 published examples of CDC device, although I am not sure if any of them uses the library you want.
0 件の賞賛
返信