Redsuite 5 license support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Redsuite 5 license support

1,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by George Chen on Thu Jul 02 18:33:44 MST 2015
I received in response to NXP forum to do on Monday and Wednesday (Taiwan time)
1. First deactive license again active license, is failure
2. First delect CDM file again active license, is failure.
and recevied response if has any problem contac [email protected].
I on Tuesday and Thursday (Taiwan time) to send a letter to [email protected], but did not receive any response, and now I should contact for assistance with which unit


Case #: 00061827_ref:_00D20NBgb._500D0ySrjw:ref
Case #: 00061845_ref:_00D20NBgb._500D0yTAUx:ref

Thank you
0 件の賞賛
返信
3 返答(返信)

1,244件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 03 01:09:20 MST 2015
Please DO NOT post email addresses. These are harvested by robots and greatly increase the amount of spam we receive. Please edit your posts to remove the email addresses.

We have now received your email and responded.
0 件の賞賛
返信

1,244件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by George Chen on Fri Jul 03 00:52:00 MST 2015
Hello

Thank you reply,
Can I double check the E-mail address is <removed>
0 件の賞賛
返信

1,244件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 03 00:32:08 MST 2015
No such email has been received at code-red-tech.com, which is why you have not received a reply.

Please note that the same people answer all questions on LPCXpresso and Red Suite, however the question is received. So the answer you receive from the two cases you quote are correct. You will not get a different reply by emailing code-red-tech.
0 件の賞賛
返信