Redsuit IDE and Red Probe Emulator support needed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Redsuit IDE and Red Probe Emulator support needed

2,016 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dhanapal_2005 on Fri Jul 17 00:28:33 MST 2015
Dear NXP Team,

Currently I am using Red Suite (NXP Edition) v4.2.3_379 IDE Licensed version and License type: FULL, Debug limit: 256k also i am using  Red Probe+ emulator.

I want to migrate from Red Suit to LPCXpresso v7.8.0_426. I have following queries.

1. Currently I am using win XP, In order to use LPCXpresso i need to update my OS to win 7. After updating windows 7, Is it possible to reactivate the current redsuit license in win 7. Reason for the need of redsuit is "Field machines are having bootloader with Red Suit so we need to give support for that"

2. Will LPCXpresso IDE support for Red Probe + Emulator?

Please give your comments.

Regards
R.Dhanapal
0 Kudos
Reply
5 Replies

1,990 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 17 05:45:50 MST 2015
Looks like you are running on XP. We do not support XP with recent versions of LPCXpresso (last version that supported XP was 7.0.2)
0 Kudos
Reply

1,989 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dhanapal_2005 on Fri Jul 17 05:29:04 MST 2015
Team,

Using LPCXpresso v7.8.0_426 through Red Probe+  i tried to connect the Target. It is not connecting. Please help me to get out of this.

When target discovery fails then timeout is not happening in LPCXpresso v7.8.0_426(I need to close the entire LPCXpresso IDE). Please find the attached screenshot.

Regards
R.Dhanapal
0 Kudos
Reply

1,989 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Fri Jul 17 04:15:21 MST 2015
Farnell are never cheap for anything.

€15 from Embedded Artists:
http://www.embeddedartists.com/products/lpcxpresso/lpclink2.php
0 Kudos
Reply

1,989 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Jul 17 03:36:18 MST 2015
In the UK, Farnell want 18 GB pounds for the LPC-Link2.


That's some exchange rate!
0 Kudos
Reply

1,989 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 17 01:00:02 MST 2015
1. Yes. See
http://support.code-red-tech.com/CodeRedWiki/MovingLicenses
2. Yes. But I would strongly recommend upgrading to LPC-Link2 - which cost about $20 each.
0 Kudos
Reply